About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

Jump to solution
1,349 Views
yuuki
Senior Contributor II

Dear all,

We were estimating KK4.4.2 on the SABRE-SD board.

AndroidKK4.4.3 was released on the Web site of Freescale, so we're trying that.

However, the file configuration of the Bootloader is changed from KK4.4.2.

Could you teach the file doing parameter setting of DDR and PHY?
(File name and location)

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
1,238 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
4 Replies
1,239 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,238 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

Android KK4.4.3 is based on Linux 3.10.53 kernel,

in kernels with device tree dcd data (setting of DDR) is defined in file

ubootxx/board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,238 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

We were able to find a file for mx6dl and mx6solo.
However, we were not able to find a file for mx6quad.

Do we have to make a file for mx6quad?

Best Regards,
Yuuki

0 Kudos
Reply
1,238 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply