About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About parameter setting of AndroidKK4.4.3 for i.MX6Q_SABRE-SD

ソリューションへジャンプ
1,325件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We were estimating KK4.4.2 on the SABRE-SD board.

AndroidKK4.4.3 was released on the Web site of Freescale, so we're trying that.

However, the file configuration of the Bootloader is changed from KK4.4.2.

Could you teach the file doing parameter setting of DDR and PHY?
(File name and location)

Best Regards,
Yuuki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,214件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,215件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,214件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

Android KK4.4.3 is based on Linux 3.10.53 kernel,

in kernels with device tree dcd data (setting of DDR) is defined in file

ubootxx/board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,214件の閲覧回数
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

We were able to find a file for mx6dl and mx6solo.
However, we were not able to find a file for mx6quad.

Do we have to make a file for mx6quad?

Best Regards,
Yuuki

0 件の賞賛
返信
1,214件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信