About package installation of glid2 for LTIB of MX6LinuxBSP
Environment is the following.
- MCIMX6DL-SDP
- L3.0.35_4.1.0_ER_SOURCE_BSP
We would like to incorporate gstreamer.
However, the following error occurs.
"import is needed by glib2-2.22.1-1"
Would you teach the method for solving this error?
Beset Regards,
已解决! 转到解答。
Hi yuuki, do you have solved this error ? when I build Qt by ltib , the same error occurs:
Processing: glib2
===================
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' glib2 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/Carl/LTIB/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/Carl/LTIB/ltib/rpm/RPMS/arm/glib2-2.22.1-1.arm.rpm
error: failed dependencies:
import is needed by glib2-2.22.1-1
BSP:
L3.0.35_4.1.0_ER_SOURCE_BSP
Yuuki
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing