About internal data flow in case of still image JPEG save.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About internal data flow in case of still image JPEG save.

跳至解决方案
1,230 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I'd like to know the internal data flow in case of still image JPEG save.

Camera --> CSI --> ?? --> SD card

[OS: Linux L3.0.35_4.1.0]

Or, give me the document about internal data flow with camera capture.

Keita

标签 (4)
0 项奖励
回复
1 解答
1,151 次查看
Yuri
NXP Employee
NXP Employee

Since i.MX6 VPU does not support JPEG, assuming software codec operations (or data from cam is JPEG coded),

the following scheme may be applied :

Camera --> CSI --> SMFC (Sensor Multi FIFO) --> IDMAC --> memory --> SD card


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,152 次查看
Yuri
NXP Employee
NXP Employee

Since i.MX6 VPU does not support JPEG, assuming software codec operations (or data from cam is JPEG coded),

the following scheme may be applied :

Camera --> CSI --> SMFC (Sensor Multi FIFO) --> IDMAC --> memory --> SD card


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复