Kernel Panic - Internal Error: Oops: 5 with SECO iMX6 uQ7 DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel Panic - Internal Error: Oops: 5 with SECO iMX6 uQ7 DL

2,015 次查看
anupkini
Contributor I

Dear All,

I have newly started working on the iMX6 Dual Lite micro-Q7 board from SECO.

I have built a yocto layer with the following details:

DEFAULTTUNE="cortexa9hf-neon"

MACHINE_FEATURES += " usbhost ethernet wifi bluetooth pci"

When i try to boot the uImage built using the above features, i end up with a kernel panic.

[    1.006121] Unable to handle kernel NULL pointer dereference at virtual address 00000001

[    1.014238] pgd = 80004000

[    1.016953] [00000001] *pgd=00000000

[    1.020555] Internal error: Oops: 5 [#1] PREEMPT SMP

Detailed bootlog here: iMX6-DL-uQ7-SECO - Pastebin.com

I am able to build the uImage with arm-fsl-linux-gnueabi.

So, the linux sources are working and no issues there.

Kindly have a look and let me know where i am going wrong.

Thanks,
Anup.

标记 (3)
0 项奖励
回复
1 回复

1,147 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 项奖励
回复