About imx8mm mipi write interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About imx8mm mipi write interface

1,913 Views
13660284951
Contributor III

hello:nxp friends?

    I had some questions with imx8mm on android9 platform?

No1: use 《 mipi_dsi_dcs_write_buffer() 》 this interface write lcd parasm,while i found,it can not long write?

No2:while use uuu to download firmware to emmc on ubuntu18,the adb and fastboot is ok,while it return error with log is "FB:ucmd setenv fastboot_dev mmc"

 

0 Kudos
Reply
4 Replies

1,818 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhou

seems rm67191 driver have dcs long write for backlight brightness setting

function mipi_dsi_dcs_set_display_brightness() :

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

>The imx8mm manual told us imx8mm is no longer supported framebuffer device,use drm instead?

please check Linux 5.4.3_1.0.0 Documentation  for supported functionality.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,818 Views
13660284951
Contributor III

thanks igorpadykov

    I had a question,when i call  mipi_dsi_dcs_write_buffer() interface to write cmd data,it return 0 to us not erro code?

what happen?

 

while call mipi_dsi_dcs_read() interface to read lcd id,that return 1 byte correct value to us?

 

what happen? @igorpadykov

 

i was confused

0 Kudos
Reply

1,818 Views
13660284951
Contributor III

thanks igorpadykov

    I had a question,when i call  mipi_dsi_dcs_write_buffer() interface to write cmd data,it return 0 to us not erro code?

what happen?

while call mipi_dsi_dcs_read() interface to read lcd id,that return 1 correct to us?

what happen? @igorpadykov

i was confused

0 Kudos
Reply

1,818 Views
13660284951
Contributor III

By the way

No1:The imx8mm manual told us imx8mm is no longer supported framebuffer device,use drm instead?

so the log

     [    1.300514] Unable to create device for framebuffer 0; errno = -19

is ring way?

And  sysfs in /dev or /class/sys/graphics are not created fbx device node

0 Kudos
Reply