About i.MX7Dual DDR Routing Rules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX7Dual DDR Routing Rules

Jump to solution
2,071 Views
felixhsu
Contributor III

Hi All

Due to i.MX7 layout review check list isn’t released, we provide i.MX6 check list for customer now.

 

But some layout rules are conflict between i.MX6 and i.MX7.

 

For example, i.MX6 check list-DRAM bus length check.

 

It says” the maximum length difference should be less than 25 mils”.

 

But at i.MX6 Hardware development guide, it shows +/-25mils is acceptable.

 

So the rule in i.MX6 check list seems to be more strictly.

 

Our question is we read i.MX7 Hardware development guide.

 

The rule it shows is +/- 55 mils.

 

Is it the right value for i.MX7 DDR trace length check?

 

Or we should follow i.MX6 check list to do this layout of DDR circuit.

Thanks.

i.mx6ddr_routing.png

i.mx7ddr_routing.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,835 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX7 DDRC is not the same as i.MX6 MMDC, therefore please use the Hardware

Development Guide for i.MX7.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
Reply
1 Reply
1,836 Views
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX7 DDRC is not the same as i.MX6 MMDC, therefore please use the Hardware

Development Guide for i.MX7.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply