About i.MX7Dual DDR Routing Rules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About i.MX7Dual DDR Routing Rules

ソリューションへジャンプ
2,056件の閲覧回数
felixhsu
Contributor III

Hi All

Due to i.MX7 layout review check list isn’t released, we provide i.MX6 check list for customer now.

 

But some layout rules are conflict between i.MX6 and i.MX7.

 

For example, i.MX6 check list-DRAM bus length check.

 

It says” the maximum length difference should be less than 25 mils”.

 

But at i.MX6 Hardware development guide, it shows +/-25mils is acceptable.

 

So the rule in i.MX6 check list seems to be more strictly.

 

Our question is we read i.MX7 Hardware development guide.

 

The rule it shows is +/- 55 mils.

 

Is it the right value for i.MX7 DDR trace length check?

 

Or we should follow i.MX6 check list to do this layout of DDR circuit.

Thanks.

i.mx6ddr_routing.png

i.mx7ddr_routing.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,820件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX7 DDRC is not the same as i.MX6 MMDC, therefore please use the Hardware

Development Guide for i.MX7.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX7 DDRC is not the same as i.MX6 MMDC, therefore please use the Hardware

Development Guide for i.MX7.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信