About boot flow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,749件の閲覧回数
goto11
Contributor III

hello,Community


Figure 6-46 SD / MMC manufacture boot flow of i.MX 7 Dual Applications Processor Reference Manual is described in the reference manual.
For example, in the case of internal boot setting, if primary boot (for example, QSPI setting) fails, it proceeds to SDMMC MFG mode judgment.
After that, the default value is enable, so proceed to SDMMC MFG mode boot.
In SDMMC MFG mode boot, do you check boot sequentially from USDHC-1 to USDHC-3 regardless of how the allocation of USDHC is (SD or other than SD)?

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,674件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  In the manufacture mode, the SD or MMC card will be scanned on the uSDHC1.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,675件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  In the manufacture mode, the SD or MMC card will be scanned on the uSDHC1.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信