About Boot from QuadSPI (BOOT_CFG)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Boot from QuadSPI (BOOT_CFG)

1,774 Views
goto11
Contributor III

hello,Community


The READ or WRITE sequence on the memory side during BOOT differs depending on whether the flash memory side is set to standard SPI or QSPI.
If the Boot QuadSPI configuration parameters are stored in the flash memory, how can the configuration be read from the flash memory even though the flash memory setting is standard SPI or QSPI is not known? .

best regards

Goto

Labels (1)
0 Kudos
Reply
3 Replies

1,701 Views
goto11
Contributor III

hello,

Can the first “ROM reads configuration parameters using the default read command” be able to read external flash memory settings using standard SPI or QSPI?

best regards

Goto

0 Kudos
Reply

1,700 Views
Yuri
NXP Employee
NXP Employee

Yes, the QSPI can be read after reset using the default read command.

~Yuri.

0 Kudos
Reply

1,701 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  According to section 6.6.6.2 (QuadSPI serial flash BOOT operation) of i.MX 7Dual

Reference Manual, Rev. 1, 01/2018, the QuadSPI interface initialization is a two-step process.

At first, the ROM reads configuration parameters using the default read command configured in

the LUT of the QuadSPI interface with the SCLOCK operating at 20 MHz.

  Note, BOOT_CFG[15:12] define if Boot from QuadSPI is selected.  

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply