About boot flow

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About boot flow

跳至解决方案
1,190 次查看
goto11
Contributor III

hello,Community


Figure 6-46 SD / MMC manufacture boot flow of i.MX 7 Dual Applications Processor Reference Manual is described in the reference manual.
For example, in the case of internal boot setting, if primary boot (for example, QSPI setting) fails, it proceeds to SDMMC MFG mode judgment.
After that, the default value is enable, so proceed to SDMMC MFG mode boot.
In SDMMC MFG mode boot, do you check boot sequentially from USDHC-1 to USDHC-3 regardless of how the allocation of USDHC is (SD or other than SD)?

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,115 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  In the manufacture mode, the SD or MMC card will be scanned on the uSDHC1.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,116 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  In the manufacture mode, the SD or MMC card will be scanned on the uSDHC1.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复