About bit swapping of data lanes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About bit swapping of data lanes

ソリューションへジャンプ
2,154件の閲覧回数
okamotosatoshi
Contributor IV

Hi There,

I am designing LPDDR4 using i.MX8M Mini.

 

i.MX6 has the following restrictions on the data lane.

 ・D0, D8, D16, D24, D32, D40, D48, and D56 are fixed
 ・Other data lines free to swap within byte lane
  (Refer to the Hardware Development Guide)

 

i.MX8M Mini has the following description.

 ・Byte swapping within each 16-bit channel is OK. Bit swapping within each slice/byte lane is OK.
  (Refer to the Hardware Developer's Guide)

 

Is it okay to think that i.MX8M Mini has no restrictions to fix the lower bits ?

 

Best regards
- satoshi

0 件の賞賛
返信
1 解決策
2,147件の閲覧回数
Yuri
NXP Employee
NXP Employee

@okamotosatoshi 

Hello,

   Yes, i.MX8M Mini has no restrictions to fix the lower bits.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,143件の閲覧回数
okamotosatoshi
Contributor IV

Hi Yuri

 

Thank you for your answer!

I understand that there are no restrictions to fix the lower bits.

I consider pin swaps according to the guidelines.

 

Best regards
- satoshi

0 件の賞賛
返信
2,148件の閲覧回数
Yuri
NXP Employee
NXP Employee

@okamotosatoshi 

Hello,

   Yes, i.MX8M Mini has no restrictions to fix the lower bits.

Regards,
Yuri.

0 件の賞賛
返信