About adjustment function of SDHC in i.MX6SDL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About adjustment function of SDHC in i.MX6SDL.

1,145 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about adjustment function of SDHC in i.MX6SDL.

I got the information that i.MX6 has Variable_Output_Data_Window(CMD19) function from below URL.

https://community.freescale.com/thread/334945

[Question]

[Q1]

When the adjustment specification of the SD card is tOP = 0~2[UI], is it possible to adjust regardless of the relation with the propagation-delay-time of the clock and data?

[Q2]

How is a sample point of host side fixed (adjusted) in Variable-clock function?

There is below description in SD Phsical Layer Specification V4.20.

"At the initialization step the host should take care to find the optimal sampling point for the card outputs."

Is this adjusted for the setup and hold to become a center?

(If it's yes, how much does the looseness occur?)

Best Regards,

Keita

Labels (5)
0 Kudos
Reply
2 Replies

1,031 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

please elevate this through local FAE

(reason is that I have big difficulties to understand questions).

Thanks.

Best regards

igor

0 Kudos
Reply

1,031 Views
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Sorry for my poor question.

I will re-post this question to understand easily.

So, I'll remove this request.

BR,

Keita

0 Kudos
Reply