About a timing between Data Valid and DTACK Active in DTACK mode Read Access for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About a timing between Data Valid and DTACK Active in DTACK mode Read Access for i.MX6

跳至解决方案
1,389 次查看
yuuki
Senior Contributor II

Dear all,

We want to use DTACK mode of EIM.

We referred to the following part of the data sheet.

IMX6DLIEC.pdf (Rev.5)

- Figure 21. DTACK Mode Read Access (DAP=0)

- Table 38. EIM Asynchronous Timing Parameters Table Relative Chip to Select

We have the following question about a timing for DTACK mode Read Access.

I understand that the DTACK signal should become active after the Data valid.

Is my understanding right?

According to Figure 21,

the DTACK signal becomes active after the Data valid.

However, according to Table 38,

"Input Data Valid to EIM_CSx_B Invalid"(WE43) is Min "MAXCO - MAXCSO + MAXDI"ns.

   => MAXCO(10ns) - MAXCSO(10) + MAXDI(5ns) = 5ns

"EIM_DTACK_B Active to EIM_CSx_B Invalid"(WE47) is Min "MAXCO - MAXCSO + MAXDTI"ns.

   => MAXCO(10ns) - MAXCSO(10) + MAXDTI(10ns) = 10ns

For the timing, the Data becomes valid after DTACK active.

How should I understand the explanation of the data sheet?

May I have advice?

Best Regards,

Yuuki

标签 (2)
标记 (4)
0 项奖励
回复
1 解答
1,254 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Yes, generally DTACK is intended to indicate data valid state.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,254 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The mentioned minimal values for parameters WE43 and WE47 

are just hardware values, that does not take into account that some
EIM timings are software configurable. Say, CS0 assertion time is
defined by the RWSC bit field of EIM_CSnRCR1 register, and if RWSC

is not equal zero (quite reasonable case), minimal WE43 is not actual.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,254 次查看
yuuki
Senior Contributor II

Dear Yuri-san,

Thank you for your support.

I understand that the DTACK signal should become active after the Data valid.

Is my understanding right?

May I have advice?

Best Regards,

Yuuki

0 项奖励
回复
1,255 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Yes, generally DTACK is intended to indicate data valid state.

Regards,

Yuri.

0 项奖励
回复