Dear Sir or Madam,
Hello.
I have got the below answer about Variable delay function of SD specification in i.MX6 series.
About Variable_Output_Data_Window of SD specification in i.MX6 series.
"CMD19 is supported for both SDR-104 and SDR-50."
But, refer to Table 67-6. Commands for MMC/SD/SDIO Cards (P.5618) in IMX6DQRM(Rev.2).
"CMD19 is Reserved"
And then, refer to uSDHCx_INT_STATUS field descriptions(P.5654).
"Tuning Pass:(only for SD3.0 SDR104 mode)
Current CMD19 transfer is done successfully. That is, current sampling point is correct."
Is the tuning function supporting for both SDR-104 and SDR-50?
Best Regards,
Keita
解決済! 解決策の投稿を見る。
Hi Keita
I checked iROM sources and cmd19 is used by iROM,
so it is supported. You are right that i.MX6 supports it only
for SDR-104 as states documentation, SD 3.0 specification
leaves SDR-50 as optional.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
I checked iROM sources and cmd19 is used by iROM,
so it is supported. You are right that i.MX6 supports it only
for SDR-104 as states documentation, SD 3.0 specification
leaves SDR-50 as optional.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------