About Variable delay function of SD specification in i.MX6 series.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About Variable delay function of SD specification in i.MX6 series.

跳至解决方案
1,559 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have got the below answer about Variable delay function of SD specification in i.MX6 series.

About Variable_Output_Data_Window of SD specification in i.MX6 series.

"CMD19 is supported for both SDR-104 and SDR-50."

But, refer to Table 67-6. Commands for MMC/SD/SDIO Cards (P.5618) in IMX6DQRM(Rev.2).

"CMD19 is Reserved"

And then, refer to uSDHCx_INT_STATUS field descriptions(P.5654).

"Tuning Pass:(only for SD3.0 SDR104 mode)

Current CMD19 transfer is done successfully. That is, current sampling point is correct."

Is the tuning function supporting for both SDR-104 and SDR-50?

Best Regards,

Keita

0 项奖励
回复
1 解答
1,265 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

I checked iROM sources and cmd19 is used by iROM,

so it is supported. You are right that i.MX6 supports it only

for SDR-104 as states documentation, SD 3.0 specification

leaves SDR-50 as optional.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,266 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

I checked iROM sources and cmd19 is used by iROM,

so it is supported. You are right that i.MX6 supports it only

for SDR-104 as states documentation, SD 3.0 specification

leaves SDR-50 as optional.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复