About V5 KEY_ROW4 terminal.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About V5 KEY_ROW4 terminal.

ソリューションへジャンプ
1,640件の閲覧回数
takashitakahash
Contributor III

Hi community.

About  question of V5 KEY_ROW4 for the terminal.

In IMX6DQRM Rev 2, of  sect 36.4.375 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_KEY_ROW4) Bit # 15,14 setting value in the Reset has become a 0b10,

100K Ohm Pull Up has been selected.

On the other hand, IMX6DQAEC Rev. 3  of Table 100 Out of Reset Condition has become a PD (100K).

Since there is no in Table 101 is KEY_ROW4, in Res, is a terminal that does not change Res later state.

Which is correct the Reference manuals or data sheet ?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,603件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

correct is datasheet  IMX6DQAEC Rev. 3  of Table 100 Out of Reset Condition

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,604件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

correct is datasheet  IMX6DQAEC Rev. 3  of Table 100 Out of Reset Condition

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信