About Table 15. Low Power Measurements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About Table 15. Low Power Measurements

跳至解决方案
1,871 次查看
goto11
Contributor III

Hello,Community

About Table 15. Low Power Measurements in i.MX 7Dual Family of Applications Processors Datasheet


About power consumption of SUSPEND,
In section 4.1.6.5, the description of the SUSPEND mode states whether VDD_ARM is turned off or not.
Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?
(Because current and power values were entered in the VDD_ARM column, I thought I would not turn off VDD_ARM.)

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,769 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?

yes this is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,770 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?

yes this is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复