About Table 15. Low Power Measurements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Table 15. Low Power Measurements

ソリューションへジャンプ
1,865件の閲覧回数
goto11
Contributor III

Hello,Community

About Table 15. Low Power Measurements in i.MX 7Dual Family of Applications Processors Datasheet


About power consumption of SUSPEND,
In section 4.1.6.5, the description of the SUSPEND mode states whether VDD_ARM is turned off or not.
Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?
(Because current and power values were entered in the VDD_ARM column, I thought I would not turn off VDD_ARM.)

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,763件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?

yes this is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,764件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>Is the power consumption of SUSPEND in Table 15 when VDD_ARM is not turned off?

yes this is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信