About SDMA support for UART in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About SDMA support for UART in i.MX6DQ.

ソリューションへジャンプ
1,649件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to "46.1 Introduction" in i.MX 6 Linux Reference Manual, Rev. L3.10.17_1.0.0-ga, 05/2014

========

If you want to use the DMA support for UART please also

enable the RTS/CTS for it. The DMA may be abnormal if you

do not enable the RTS/CTS.

========

I'd like to know the why FSL judged that RTS/CTS need.

(My customer will use SDMA with UART that do not enable the RTS/CTS.)

What problem did freescale face in the past?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,305件の閲覧回数
Yuri
NXP Employee
NXP Employee

  UART interface is relatively slow, therefore special lines are required

for hardware ready acknowledgement, in order to avoid data FIFO overrun.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,306件の閲覧回数
Yuri
NXP Employee
NXP Employee

  UART interface is relatively slow, therefore special lines are required

for hardware ready acknowledgement, in order to avoid data FIFO overrun.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,305件の閲覧回数
keitanagashima
Senior Contributor I

Hi Yuri,

Thank you for your answer.

I understood the reason.

Best Regards,

Keita

0 件の賞賛
返信