About SDMA support for UART in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About SDMA support for UART in i.MX6DQ.

Jump to solution
935 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to "46.1 Introduction" in i.MX 6 Linux Reference Manual, Rev. L3.10.17_1.0.0-ga, 05/2014

========

If you want to use the DMA support for UART please also

enable the RTS/CTS for it. The DMA may be abnormal if you

do not enable the RTS/CTS.

========

I'd like to know the why FSL judged that RTS/CTS need.

(My customer will use SDMA with UART that do not enable the RTS/CTS.)

What problem did freescale face in the past?

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
591 Views
Yuri
NXP Employee
NXP Employee

  UART interface is relatively slow, therefore special lines are required

for hardware ready acknowledgement, in order to avoid data FIFO overrun.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
592 Views
Yuri
NXP Employee
NXP Employee

  UART interface is relatively slow, therefore special lines are required

for hardware ready acknowledgement, in order to avoid data FIFO overrun.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
591 Views
keitanagashima
Senior Contributor I

Hi Yuri,

Thank you for your answer.

I understood the reason.

Best Regards,

Keita

0 Kudos