About RGB-selection of SCART terminal in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About RGB-selection of SCART terminal in i.MX6DQ.

Jump to solution
1,305 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is it possible to output the RGB-selection signal in i.MX6DQ's IPU?

Refer to below link and 16 pin.

SCART - Wikipedia, the free encyclopedia

=======

Pin 16 Blanking signal up

RGB-selection voltage up

0 - 0.4 V --> composite

1 - 3 V --> RGB

=======

(My customer would like to use the external IC to overlay the two video "RGB and composite".)

Best Regards,

Keita

Labels (4)
0 Kudos
Reply
1 Solution
1,229 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

unfortunately i.MX6DQ's IPU can not produce

such kind of signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,230 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

unfortunately i.MX6DQ's IPU can not produce

such kind of signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,229 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your prompt reply!

Best Regards,

Keita

0 Kudos
Reply