Dear Sir or Madam,
Hello.
Is it possible to output the RGB-selection signal in i.MX6DQ's IPU?
Refer to below link and 16 pin.
SCART - Wikipedia, the free encyclopedia
=======
Pin 16 Blanking signal up
RGB-selection voltage up
0 - 0.4 V --> composite
1 - 3 V --> RGB
=======
(My customer would like to use the external IC to overlay the two video "RGB and composite".)
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
unfortunately i.MX6DQ's IPU can not produce
such kind of signal.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
unfortunately i.MX6DQ's IPU can not produce
such kind of signal.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your prompt reply!
Best Regards,
Keita