About Power mode transitions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Power mode transitions

Jump to solution
1,861 Views
goto11
Contributor III

Hello,Community

There are two questions about Table 6-8 Power mode transitions in i.MX 7 Dual Applications Processor Reference Manual.

(1) Does this mean that timer interrupt is enabled by LP Time Alarm Enable in SNVS_LP Control Register (LPCR)?
Which field should I check to see if an interrupt was asserted?

(2) If DP_EN of SNVS_LP Control Register (LPCR), can PMIC_ON_REQ signal be set to 0 in TOP?

Table 6-8. Is the Configuration with internal PMIC column of Power mode transitions Dumb PMIC?

Best reguards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,803 Views
igorpadykov
NXP Employee
NXP Employee

Hi GoTo

1. yes. It can be checked using SNVS_LPSR bit LPTA

2. yes it is dumb mode, usage TOP and DP_EN can be found in patch on

Q&A: How is mx6 PMIC_ON_REQ under SW control? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,804 Views
igorpadykov
NXP Employee
NXP Employee

Hi GoTo

1. yes. It can be checked using SNVS_LPSR bit LPTA

2. yes it is dumb mode, usage TOP and DP_EN can be found in patch on

Q&A: How is mx6 PMIC_ON_REQ under SW control? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply