About Power mode transitions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Power mode transitions

ソリューションへジャンプ
1,633件の閲覧回数
goto11
Contributor III

Hello,Community

About Table 6-8Power mode transitions in i.MX 7 Dual Applications Processor Reference Manual
There is "Upon alarm_in assertion to '1'" in Normal ON to OFF, by button and Configuration with internal PMIC column.
Where is the register for alarm_in?

Best reguards,

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,564件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

there is no register for alarm_in as this is internal signal, for

button power off configuration one can look at description of

SNVS_LP Control Register (LPCR) register.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,565件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

there is no register for alarm_in as this is internal signal, for

button power off configuration one can look at description of

SNVS_LP Control Register (LPCR) register.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信