About Power mode transitions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Power mode transitions

Jump to solution
1,607 Views
goto11
Contributor III

Hello,Community

About Table 6-8Power mode transitions in i.MX 7 Dual Applications Processor Reference Manual
There is "Upon alarm_in assertion to '1'" in Normal ON to OFF, by button and Configuration with internal PMIC column.
Where is the register for alarm_in?

Best reguards,

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,538 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

there is no register for alarm_in as this is internal signal, for

button power off configuration one can look at description of

SNVS_LP Control Register (LPCR) register.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,539 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

there is no register for alarm_in as this is internal signal, for

button power off configuration one can look at description of

SNVS_LP Control Register (LPCR) register.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply