About ON_TIME

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ON_TIME

2,021 Views
goto11
Contributor III

hello,Community

About ON_TIME (00: 500msec off-> on transition time)
Is the time from when BTN is asserted to when the SOC power is turned on including the time when power is supplied to the iMX and the reset release time?
Browse attachments

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Reply

1,948 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Goto,

The function of the ON_TIME is slightly different. You can see a simplified diagram on the following Community Document. The BTN must be asserted ON_TIME miliseconds so that the PMIC is asserted to power on the SoC power.

https://community.nxp.com/docs/DOC-97660

I hope this information helps!

Regards,

0 Kudos
Reply