About Non-Gated Clock Mode issue of the Parallel CSI module on the i.MX 6ULL series MPU.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Non-Gated Clock Mode issue of the Parallel CSI module on the i.MX 6ULL series MPU.

ソリューションへジャンプ
4,065件の閲覧回数
vikenzhou
Contributor I
Hi, I am have a question about the Parallel CSI module, hope here can get answer, thank you!
When MPU is running  in Non-Gated Clock Mode, because the HSYNC signal will be ignored,
How know a line the number of pixels, it is possible using the clock edge to latched data;  if so,  in this Parallel_CSI_TX side, the pixel data of a line can many discontinuous clock cycles to send out ?
Please see below the figure,  thank you!
0 件の賞賛
返信
1 解決策
4,059件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for non-gated mode, pls see the pic as below:

joanxie_1-1606891449510.png

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,049件の閲覧回数
vikenzhou
Contributor I

Thans for your great support, the following questions please help guide again, thank you!
1, I have to see the pictures of you reply which is included a Data_EN signal, the signal in the Parallel_CSI_RX is necessary? The figure 19 on page758 of document  (IMX6ULLRM.pdf), Here is no use this Data_EN signal.
2, When sending a line of pixels, is the need for a continuous clock to send a line, or send a line of pixels can be discontinuous .

0 件の賞賛
返信
4,060件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for non-gated mode, pls see the pic as below:

joanxie_1-1606891449510.png

 

 

0 件の賞賛
返信
4,037件の閲覧回数
vikenzhou
Contributor I

Why in rev.1 Reference Manual there is no Data_EN .

0 件の賞賛
返信
4,045件の閲覧回数
vikenzhou
Contributor I
 
0 件の賞賛
返信