About LPDDR3 command and address timing diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LPDDR3 command and address timing diagram

Jump to solution
1,209 Views
goto11
Contributor III

Hello,Community

I have two questions.
1.Figure 27 in i.MX 7 Dual Family of Applications Processors Datasheet, Rev. 6
LP5 and LP6 are missing in Table 50. LPDDR3 timing parameters.
Please tell me the parameter value.

2.There is a description of the DRAM_CAS_B signal, but there is no such signal in the LPDDR3 signal.
Is it an address signal?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,083 Views
karangajjar
Senior Contributor II

Hi goto11@wantsinc.jp,

It would be better if you refer JEDEC standard for LPDDR3 timings parameters. 

Also, we believe there is a typo in case of DRAM_CAS_B, there is no CAS signal in case of LPDDR3. There should be

DRAM_CAx (command and address bus).

Regards,

Karan Gajjar

View solution in original post

0 Kudos
Reply
1 Reply
1,084 Views
karangajjar
Senior Contributor II

Hi goto11@wantsinc.jp,

It would be better if you refer JEDEC standard for LPDDR3 timings parameters. 

Also, we believe there is a typo in case of DRAM_CAS_B, there is no CAS signal in case of LPDDR3. There should be

DRAM_CAx (command and address bus).

Regards,

Karan Gajjar

0 Kudos
Reply