About LPDDR2 Script Aid Options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About LPDDR2 Script Aid Options

1,566件の閲覧回数
tony_l_cai
Contributor III

Hi, All

       in LPDDR2 Script Aid,how can I fill in these blanks? some configuration options below:

PCB Parameters
DRAM DSE Setting - DQ/DQM (ohm)40
DRAM DSE Setting - CA/CTL (ohm)40
DRAM DSE Setting - CK (ohm)48
DRAM DSE Setting - DQS (ohm)40

And I have read the user guide for DDR3, but in this guide, no more details about these parms,just " SI design experience or simulation result ",please give  me more info , thanks!

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 返信

1,382件の閲覧回数
Yuri
NXP Employee
NXP Employee

  You may try to adjust drive strength settings experimentally, using different
options and memory test. Also, You may look at waveforms of the corresponding
signals, if they do not have voltage over-/under-shoots.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信