About LPDDR2 Script Aid Options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LPDDR2 Script Aid Options

1,607 Views
tony_l_cai
Contributor III

Hi, All

       in LPDDR2 Script Aid,how can I fill in these blanks? some configuration options below:

PCB Parameters
DRAM DSE Setting - DQ/DQM (ohm)40
DRAM DSE Setting - CA/CTL (ohm)40
DRAM DSE Setting - CK (ohm)48
DRAM DSE Setting - DQS (ohm)40

And I have read the user guide for DDR3, but in this guide, no more details about these parms,just " SI design experience or simulation result ",please give  me more info , thanks!

Labels (2)
0 Kudos
Reply
1 Reply

1,423 Views
Yuri
NXP Employee
NXP Employee

  You may try to adjust drive strength settings experimentally, using different
options and memory test. Also, You may look at waveforms of the corresponding
signals, if they do not have voltage over-/under-shoots.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply