About HDMI Tx HDCP encryption in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About HDMI Tx HDCP encryption in i.MX6DQ.

1,437 次查看
keitanagashima
Senior Contributor I

Dear All,

About HDMI TX HDCP encryption, mycustomer is using the i.MX 6Dual with enabled HDCP (SC part number).

And, they can get "HDCP engaged" (i.e. video is encrypted successfully).

To further verify the encryption function, we'd like to know:

1) How can we check whether the video which output by HDMI TX has been indeed encrypted?

2) If we want to output encrypted video to a Sink device which does not support HDCP decryption,how can we get such Sink device?

3) If we want to output encrypted video to a Sink device whose HDCP private key is illegal,how can we get such Sink device?

Do you have some methods to test these situation?

Or how can we get such special test device?

[BSP: L3.0.35_4.1.0]

Best Regards,

Keita

标签 (3)
0 项奖励
回复
4 回复数

1,234 次查看
keitanagashima
Senior Contributor I

Hi Yuri,

OK. I got it.

I created the new SR.

Best Regards,

Keita

0 项奖励
回复

1,234 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Sorry, but the information you are requesting is treated as confidential info at this time

and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss

this with you in public anyway, this requires to be handled as a Service Request (SR).

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 项奖励
回复

1,234 次查看
keitanagashima
Senior Contributor I

Dear Yuri,

Hello. Thank you for your reply.

OK. I got it.

> this requires to be handled as a Service Request (SR).

Should I make new SR?

Or, will you create the new SR?

Best regards,

Keita

0 项奖励
回复

1,234 次查看
Yuri
NXP Employee
NXP Employee

Hi,

Yes, You can create SR How to submit a new question for NXP Support

or

apply to local NXP representative.

Regards,

Yuri.

0 项奖励
回复