About GPU and linux GUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About GPU and linux GUI

1,984 Views
jiongzhongliu
Contributor III

I use linux 3.10 on IMX6Q,but there is problem,the GPU do not initialize success, and the linux can not go to the runlevel 5,and have the problem" /etc/init.d/rc_mxc.s line 1 command line not found".and the  kernel auto into the runlevel 3. The command line the uboot give to the kernel is right.Is GPU initialize failed can caused this problem?22.jpg

Labels (2)
0 Kudos
Reply
2 Replies

1,836 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

please use latest L4.1.15_1.1.0, as it fixed many gpu errata

(one can find description in Release Notes) :

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,836 Views
jiongzhongliu
Contributor III

hi igorpadykov:

           Thank you respond my problem! The L4.1.15 is the linux 4.1 image ,but I used the IMX6Q's trustzone function, my linux kernel is 3.10,and How can I get the linux 3.10 source that had fixed the gpu errata?

            thank you !

0 Kudos
Reply