About GPU and linux GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About GPU and linux GUI

2,014件の閲覧回数
jiongzhongliu
Contributor III

I use linux 3.10 on IMX6Q,but there is problem,the GPU do not initialize success, and the linux can not go to the runlevel 5,and have the problem" /etc/init.d/rc_mxc.s line 1 command line not found".and the  kernel auto into the runlevel 3. The command line the uboot give to the kernel is right.Is GPU initialize failed can caused this problem?22.jpg

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,866件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jiongzhong

please use latest L4.1.15_1.1.0, as it fixed many gpu errata

(one can find description in Release Notes) :

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,866件の閲覧回数
jiongzhongliu
Contributor III

hi igorpadykov:

           Thank you respond my problem! The L4.1.15 is the linux 4.1 image ,but I used the IMX6Q's trustzone function, my linux kernel is 3.10,and How can I get the linux 3.10 source that had fixed the gpu errata?

            thank you !

0 件の賞賛
返信