About Discovered Bad Block table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Discovered Bad Block table

Jump to solution
1,664 Views
takashitakahash
Contributor III

Dear community.

IMX6DQ RM 8.5.2.4 Discovered Bad Block Table, Table 8-13.

DBBT Structure to have been described as 4 * PageSize, What are the Page Size of definition here?

Is this for RAW NAND Flash page in the main area (for example 2048 Byte) bytes or total bytes including the Spare area?

(Example: 2048 +64 = 2112 Bytes).

Labels (2)
0 Kudos
Reply
1 Solution
1,574 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

page size will be 2112 Bytes ( including the spare area), for

example this is shown on Figure 8-8. Valid Layout for 2112

bytes Sized Page IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,575 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

page size will be 2112 Bytes ( including the spare area), for

example this is shown on Figure 8-8. Valid Layout for 2112

bytes Sized Page IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply