About Discovered Bad Block table

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Discovered Bad Block table

ソリューションへジャンプ
1,660件の閲覧回数
takashitakahash
Contributor III

Dear community.

IMX6DQ RM 8.5.2.4 Discovered Bad Block Table, Table 8-13.

DBBT Structure to have been described as 4 * PageSize, What are the Page Size of definition here?

Is this for RAW NAND Flash page in the main area (for example 2048 Byte) bytes or total bytes including the Spare area?

(Example: 2048 +64 = 2112 Bytes).

ラベル(2)
0 件の賞賛
返信
1 解決策
1,570件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

page size will be 2112 Bytes ( including the spare area), for

example this is shown on Figure 8-8. Valid Layout for 2112

bytes Sized Page IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,571件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

page size will be 2112 Bytes ( including the spare area), for

example this is shown on Figure 8-8. Valid Layout for 2112

bytes Sized Page IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信