About CodeAurora

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,424件の閲覧回数
funatsu
Contributor I

Hi all,

I have a question about CodeAurora.

According to the following two threads,

https://community.nxp.com/thread/323782

https://community.nxp.com/thread/499539

CodeAurora is the Freescale Official Release BSP and it is static, does not include bug fixes, apparently.

However, it seems https://source.codeaurora.org/external/imx is updated frequently.

I am going to use i.mx8 mini but I cannot see which BSPs I should use,

I mean I don't know which of the following repositories I should use,

https://github.com/Freescale/fsl-community-bsp-platform

https://source.codeaurora.org/external/imx

Can anyone tell me the difference between them?

ラベル(2)
0 件の賞賛
返信
1 解決策
4,134件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takao

>However, it seems https://source.codeaurora.org/external/imx is updated frequently.

right, for example one can look at "commits" :

pastedImage_2.jpg

 

>I am going to use i.mx8 mini but I cannot see which BSPs I should use,

supported processors are listed in Release Notes document p.1 available on

documentation link i.MX Software and Development Tools | NXP 

>I mean I don't know which of the following repositories I should use,

it is necessary to use source.codeaurora.org/external/imx/linux-imx  repository

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,134件の閲覧回数
funatsu
Contributor I

Hi igor

Thank you for your answer.

0 件の賞賛
返信
4,135件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takao

>However, it seems https://source.codeaurora.org/external/imx is updated frequently.

right, for example one can look at "commits" :

pastedImage_2.jpg

 

>I am going to use i.mx8 mini but I cannot see which BSPs I should use,

supported processors are listed in Release Notes document p.1 available on

documentation link i.MX Software and Development Tools | NXP 

>I mean I don't know which of the following repositories I should use,

it is necessary to use source.codeaurora.org/external/imx/linux-imx  repository

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信