Installing platform drivers to iMXRT project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing platform drivers to iMXRT project

1,388件の閲覧回数
gredpath
Contributor III

I am trying to generate board\pin_mux.c & .h using mex file and pins tool.

I comes up with an error telling me that I need resource platform.drivers.common, platform.drivers.iomuxc and platform.drivers.igpio

The project has obviously not been created properly, can I add these files or a path at this stage.

My colleague has directly edited the pinmux.c files ( not a good idea I know) but can I create this without completely regenerating the project?

Thanks in Advance

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,318件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi George Redpath,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I was wondering if you can present the error messages via screenshot , otherwise, I can't get an intuitive overview of the error actually.
In further, I'll appreciate it a lot if you can upload the mex file.

Looking forward to your reply.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信