About CS1 on Port A of QuadSPI configuration parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About CS1 on Port A of QuadSPI configuration parameters

Jump to solution
3,245 Views
goto11
Contributor III

Hello,

 

I am using QSPI_A to access memory.
Since the QSPI_A_SS0_B and QSPI_A_SS1_B signals are Chip select1 port0/1 deviceA, shouldn't CS1 on Port A be set to enable?
The designer says that CS1 on Port A can be accessed with the disable setting.
Is there any problem with this setting?

 

Regards,

Goto

Labels (1)
0 Kudos
Reply
1 Solution
3,211 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply
7 Replies
3,236 Views
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,


   QSPI_A_SS0_B may be used without QSPI_A_SS1_B.
Section 10.2.8.2 (Dual Die Flashes) of i.MX 7Dual Reference
Manual (Rev. 1, 01/2018) describes configuration, where
both signals are applied.

 

Regards,
Yuri.

0 Kudos
Reply
3,232 Views
goto11
Contributor III

Hello,

 

It's not the answer to what I asked.
Is the QSPI_A_SS0_B(QSPI_A_SS1_B) signal valid when the CS1 on Port A setting in Table 6-50 (QuadSPI configuration parameters) is disabled?

Regards,

Goto

0 Kudos
Reply
3,230 Views
Yuri
NXP Employee
NXP Employee

@goto11 

  The QSPI_A_SS0_B signal is valid when the CS1 on Port A setting in QuadSPI configuration parameters is disabled. QSPI_A_SS1_B is not configured for QSPI in such case.

~Yuri.

0 Kudos
Reply
3,225 Views
goto11
Contributor III

Hello,

When the setting value of "CS1 on Port A" in Table 6-50 (QuadSPI configuration parameters) is disabled, is it not possible to use Flash A2 with the following configuration?

無題.png

Regards,

Goto

0 Kudos
Reply
3,221 Views
Yuri
NXP Employee
NXP Employee

@goto11 

 if "CS1 on Port A" in  QuadSPI configuration parameters is disabled, 
it is not possible to use the Flash A2.

0 Kudos
Reply
3,219 Views
goto11
Contributor III

If the setting value of "CS1 on Port A" in Table 6-50 (QuadSPI configuration parameters) is enable, can Flash A2 with the following configuration be used?

0 Kudos
Reply
3,212 Views
Yuri
NXP Employee
NXP Employee

@goto11 

 

  yes.

0 Kudos
Reply