About BSP version described in Errata sheet for i.MX6Quad

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About BSP version described in Errata sheet for i.MX6Quad

1,015 次查看
yuuki
Senior Contributor II

Dear all,

We refer to the following Erratasheet for  i.MX6D/Q.

http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

We found the following description

"Linux BSP Status:
Software workaround implemented in BSP version ER3"

"Linux BSP Status:
Software workaround to be applied in a future BSP release"

We have some LinuxBSP.

- fsl-yocto-3.10.17_1.0.0.tar
- fsl-yocto-3.10.53-1.1.0.tar.gz
- L3.0.35_4.1.0_130816_source.tar.gz
- L3.0.101_4.1.1_141016_source.tar.gz

<Q1>
Which BSP does "BSP version ER3" mean?

<Q2>
Is the "future BSP release" included in above BSP?

Best Regards,
Yuuki

标签 (4)
标记 (1)
0 项奖励
回复
2 回复数

851 次查看
joanxie
NXP TechSupport
NXP TechSupport

as I known, kernel L3.0.35 is ER6, ER3 maybe L3.0.15 or older version.

this is the latest errata document, if this issue hasn't fixed, I think the bsp you download hasn't fixed this issue yet.

0 项奖励
回复

851 次查看
yuuki
Senior Contributor II

Dear Guanqiong Xie-san,

Thank you for your support.

For ERR007006, ERR007007, ERR007008
"Software workaround to be applied in a future BSP release" is listed in Linux BSP Status of these errata.

We have an additional question.

(1)
I think that it is necessary for these Errata to be supported on the compiler side.
Is there the planned compiler (tool) on supporting these?

(2)
Can we take measures by revising BSP without a correction on the compiler side?

May I have advice?

Best Regards,
Yuuki

0 项奖励
回复