About ADC input impedance of i.MX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ADC input impedance of i.MX25

Jump to solution
2,224 Views
yuuki
Senior Contributor II

Dear all,

Would you teach the input impedance value for ADC ports of i.MX253?
(Max value and Min value)


We investigate the output resistance value of the external device connected to ADC port.
We investigate a measurement error when we changed the output resistance from 10 Ω to 100kΩ.

Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,892 Views
art
NXP Employee
NXP Employee

Actually, the input impedance of the i.MX25 ADC is not strictly specified. However, it is specified in the i.MX25 Data Sheet that the output impedance of a signal source to measure with this ADC must not exceed 1500 Ohm to guarantee the specified measurement accuracy of +/- 0.75 LSB DNL and +/- 2.0 LSB INL.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,893 Views
art
NXP Employee
NXP Employee

Actually, the input impedance of the i.MX25 ADC is not strictly specified. However, it is specified in the i.MX25 Data Sheet that the output impedance of a signal source to measure with this ADC must not exceed 1500 Ohm to guarantee the specified measurement accuracy of +/- 0.75 LSB DNL and +/- 2.0 LSB INL.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,892 Views
yuuki
Senior Contributor II

Dear Artur-san,

Thank you for your support.

I think that the Max 1500Ohm is specification for Touchscreen.

Do INAUX0:2 pins have specification same as this, too?

Best Regards,

Yuuki

0 Kudos
Reply
1,892 Views
art
NXP Employee
NXP Employee

Yes, all of the ADC inputs of i.MX25 have the same specifications.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------