Hi-Z_FOR_BOOT_B in SABRE AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi-Z_FOR_BOOT_B in SABRE AI

Jump to solution
2,432 Views
jeevanmahadevu
Contributor II

Why  Hi-Z_FOR_BOOT_B is provided during the boot only for Touch interrupt, Magnetometer interrupt, GPS interrupt, UART3_RTS of Bluetooth and for USB_HOST, Not for any other peripherals ?

1 Solution
2,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

because these signals are connected to boot configuration

lines, like EIM_EB1(COMPASS_INT) on p.9 SPF-27142

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,323 Views
jeevanmahadevu
Contributor II

Thank you very much igor

0 Kudos
Reply
2,324 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeevan

because these signals are connected to boot configuration

lines, like EIM_EB1(COMPASS_INT) on p.9 SPF-27142

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------