About ADC channel assignment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About ADC channel assignment

跳至解决方案
1,270 次查看
goto11
Contributor III

Hello,Community

Assigned to ADC1_IN0 to ADC1_IN3 in Table 99 of the data sheet.


On the other hand, in the ADC memory map of Reference Manual, ADC1 has CH_A to CH_D.
Is it possible to assign Channel 0 to CHA_SEL, Channel 1 to CHB_SEL, Channel 2 to CHC_SEL, and Channel 3 to CHD_SEL to support the following?

IN0-CH_A
IN1-CH_B
IN2-CH_C
IN3-CH_D

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,205 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes this is possible. As described in sect.14.1.1 Overview

i.MX 7Dual Applications Processor Reference Manual

"ADC supports conversion up to five logic groups (ChA /
ChB / ChC / ChD / SW). Each group can select one channel
from 0 - 15 physical channels."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,206 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes this is possible. As described in sect.14.1.1 Overview

i.MX 7Dual Applications Processor Reference Manual

"ADC supports conversion up to five logic groups (ChA /
ChB / ChC / ChD / SW). Each group can select one channel
from 0 - 15 physical channels."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复