About ADC channel assignment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ADC channel assignment

Jump to solution
2,541 Views
goto11
Contributor III

Hello,Community

Assigned to ADC1_IN0 to ADC1_IN3 in Table 99 of the data sheet.


On the other hand, in the ADC memory map of Reference Manual, ADC1 has CH_A to CH_D.
Is it possible to assign Channel 0 to CHA_SEL, Channel 1 to CHB_SEL, Channel 2 to CHC_SEL, and Channel 3 to CHD_SEL to support the following?

IN0-CH_A
IN1-CH_B
IN2-CH_C
IN3-CH_D

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
2,475 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes this is possible. As described in sect.14.1.1 Overview

i.MX 7Dual Applications Processor Reference Manual

"ADC supports conversion up to five logic groups (ChA /
ChB / ChC / ChD / SW). Each group can select one channel
from 0 - 15 physical channels."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,476 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes this is possible. As described in sect.14.1.1 Overview

i.MX 7Dual Applications Processor Reference Manual

"ADC supports conversion up to five logic groups (ChA /
ChB / ChC / ChD / SW). Each group can select one channel
from 0 - 15 physical channels."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,242 Views
tamotsu
Contributor V

Hello igorpadykov.

This is a solution, but I don't understand it, so I have a question.

According to the pin assignment in the datasheet, there are eight physical inputs, ADC1_IN0 to ADC2_IN3.

In the reference manual, CHA_SEL of ADCx_CH_A_CFG1 ranges from 0 to 15.

What do ADC1_INx and Channelx correspond to?
Or are they unrelated?

How should I set ADC2_IN0?

Best regards.

0 Kudos
Reply