AXI iRAM usage in IMX6 VPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AXI iRAM usage in IMX6 VPU

1,690 Views
jparrish88
Contributor IV

How was the AXI iram used for vpu? What are the A9 support routines for the VPU.  (e.g. me/mv/dbk)

Also,  Does a9 core share the AXI iram with vpu? can a9 reuse this piece of iram when vpu isn't needed?

Labels (3)
Tags (3)
0 Kudos
Reply
1 Reply

1,337 Views
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

what do you mean by "AXI iram" ?

VPU does not specially use OCRAM (though you can use it in software).

OCRAM can be used as any other memory region (for example DDR3).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply