AXI iRAM usage in IMX6 VPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AXI iRAM usage in IMX6 VPU

1,663件の閲覧回数
jparrish88
Contributor IV

How was the AXI iram used for vpu? What are the A9 support routines for the VPU.  (e.g. me/mv/dbk)

Also,  Does a9 core share the AXI iram with vpu? can a9 reuse this piece of iram when vpu isn't needed?

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

1,310件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

what do you mean by "AXI iram" ?

VPU does not specially use OCRAM (though you can use it in software).

OCRAM can be used as any other memory region (for example DDR3).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信