ARM errata patch to i.MX6 android bsp.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ARM errata patch to i.MX6 android bsp.

跳至解决方案
1,859 次查看
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6 android bsp.

We found the following patch is not applied to android_jb4.2.2_1.1.0-ga, but applied to android_kk4.4.2_1.0.0-ga.

https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/commit/?id=8404663f81d212918ff85f493...

Then, would you let me know the reason why the patch is applied to android_kk4.4.2_1.0.0-ga even though both bsp use same kernel revision (3.0.35)?

Best Regards,

Satoshi Shimoda

标签 (6)
0 项奖励
回复
1 解答
1,703 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

There was no particular reason not to include the patch in 4.2.2 other than time. According to the information I got from our specialists, it was decided not to include the patch in 4.2.2 because it was already included in 4.4.2

Please let me know if it answers your question.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,703 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

The reason is simple actually.

The patch was only applied on 4.4.2 and not from 4.2.2 because we started applying it from 4.4.2, it is just a timing issue.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,703 次查看
satoshishimoda
Senior Contributor I

Hi SerchMX,

Would you give me a reply to my additional question?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,704 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

There was no particular reason not to include the patch in 4.2.2 other than time. According to the information I got from our specialists, it was decided not to include the patch in 4.2.2 because it was already included in 4.4.2

Please let me know if it answers your question.

0 项奖励
回复
1,703 次查看
satoshishimoda
Senior Contributor I

Hi SerchMX,

Thank you for your reply.

According to your reply, we understood the patch was not released when Freescale developed android_jb4.2.2_1.1.0-ga, and it had been released when Freescale developed android_kk4.4.2_1.0.0-ga.

Is this correct?

Or Freescale did not apply the patch to android_jb4.2.2_1.1.0-ga even though the patch had been released with some reason?

(e.g. there is no enough time for estimating the effect of the patch until release android_jb4.2.2_1.1.0-ga)

Best Regards,

Satoshi Shimoda

0 项奖励
回复