ARM errata patch to i.MX6 android bsp.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM errata patch to i.MX6 android bsp.

ソリューションへジャンプ
2,046件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6 android bsp.

We found the following patch is not applied to android_jb4.2.2_1.1.0-ga, but applied to android_kk4.4.2_1.0.0-ga.

https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/commit/?id=8404663f81d212918ff85f493...

Then, would you let me know the reason why the patch is applied to android_kk4.4.2_1.0.0-ga even though both bsp use same kernel revision (3.0.35)?

Best Regards,

Satoshi Shimoda

ラベル(6)
0 件の賞賛
返信
1 解決策
1,890件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

There was no particular reason not to include the patch in 4.2.2 other than time. According to the information I got from our specialists, it was decided not to include the patch in 4.2.2 because it was already included in 4.4.2

Please let me know if it answers your question.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,890件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

The reason is simple actually.

The patch was only applied on 4.4.2 and not from 4.2.2 because we started applying it from 4.4.2, it is just a timing issue.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,890件の閲覧回数
satoshishimoda
Senior Contributor I

Hi SerchMX,

Would you give me a reply to my additional question?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,891件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Satoshi,

There was no particular reason not to include the patch in 4.2.2 other than time. According to the information I got from our specialists, it was decided not to include the patch in 4.2.2 because it was already included in 4.4.2

Please let me know if it answers your question.

0 件の賞賛
返信
1,890件の閲覧回数
satoshishimoda
Senior Contributor I

Hi SerchMX,

Thank you for your reply.

According to your reply, we understood the patch was not released when Freescale developed android_jb4.2.2_1.1.0-ga, and it had been released when Freescale developed android_kk4.4.2_1.0.0-ga.

Is this correct?

Or Freescale did not apply the patch to android_jb4.2.2_1.1.0-ga even though the patch had been released with some reason?

(e.g. there is no enough time for estimating the effect of the patch until release android_jb4.2.2_1.1.0-ga)

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信