APBH_DMA USED FOR GPMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

APBH_DMA USED FOR GPMI

1,291 次查看
michaelsyh
Contributor I

I read the ”iMX6_Firmware_Guide.pdf“, and I am curious about the DMA command structure uesd in gpmi driver, can I just use the struct "GENERIC_DESCRIPTOR" to operate the DMA channel without using the register such as next command address register.

where can I find the include files used in the test driver, and is there source code related to the code written in the ”iMX6_Firmware_Guide.pdf“?

I am really looking forward to the reply, thanks a lot!

标签 (1)
0 项奖励
回复
1 回复

1,164 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please create request in order to get the Platform SDK sources.

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复