Hello,
There is some confusion from what the MX6DL SABRE AI CPU Card schematics indicates as the recommended PMIC P/N and what the PMIC datasheet states:
Schematic (sch-27767_a_x3.pdf) and BOM (BOM-27767_A.xlsb) indicates using MMPF0100F0ZES, which has rev'd to MMPF0100F0AZES per the PMIC datasheet.
However, the PMIC datasheet (Rev. 9.0, 12/2015) recommends using the "NP" version of the part if using the MCIMX6DLAICPU1 reference design. This contradicts the AI schematic which states "F0" should be used.
From the MMPF0100Z datasheet:
From MCIMX6DLAICPU1 schematic:
What is the recommended PMIC for MCIMX6U6AVM08AC?
Thank you in advance!
Scott
Hello,
Since the non-programmed PMIC uses “NP” as the programming code - it allows
high range adaptation the NP case for customer's designs. But it may be needed
to program PMIC before using.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------